imxrt1020_evk - qspi

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imxrt1020_evk - qspi

808 Views
Oleksii
Contributor I

Please, advise a sample project to read/write/erase with QSPI memory provided on imxrt1020_evk.

Thank you in advance.

Best regards,

Oleksii

0 Kudos
Reply
1 Reply

797 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi Oleksii,

Please refer to the flexspi_nor_polling_transfer example of the SDK. In this example, flexspi will send data and operate the external Nor flash connected with FLEXSPI. Some simple flash command will be executed, such as Write Enable, Erase sector, Program page.

Have a great day,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time. 

------------------------------------------------------------------------------ 

0 Kudos
Reply