NXP LifeVibes AudioCapture

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP LifeVibes AudioCapture

1,908件の閲覧回数
abrarhuq
Contributor I

Is NXP LifeVibes AudioCapture software solution supported for i.MX 6 Series Processors (Sabre Development System)?

[NXP LifeVibes AudioCapture software solution could help with noise suppression, audio zooming, wind noise suppression to be used for tele-presence / audio conference applications]

ラベル(4)
タグ(1)
0 件の賞賛
返信
1 返信

1,821件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Abrar

please look at attached Linux Manual with description of supported

drivers, seems these features are not supported, though some processing

can be done implementing custom software.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信