NXP IMX8M Mini DDR4 Calibration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP IMX8M Mini DDR4 Calibration

2,803件の閲覧回数
DanielDuJijun
Contributor III

Dear NXP IMX Support Team;

Would you please kindly help to support to check the DDR4 Register Configuration sheets of  MX8M_Mini_DDR4_RPA_v21.xlsx is correct ?

thanks.

File list : 

1.DDR4 Datasheets : AllianceMemory_8Gb_DDR4_AS4C512M16D4_AS4C1G8D4_August2020_v1.0

2.SCH : CRP-CRA9-CoreA-V3.0

3.DDR4 RPA file : MX8M_Mini_DDR4_RPA_v21.xlsx

NXP IMX8M Mini Parts : MIMX8MM6CVTKZAA

DDR4 Parts : AS4C512M16D4-75BIN

タグ(1)
0 件の賞賛
返信
1 返信

2,788件の閲覧回数
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @DanielDuJijun,

I hope you are doing well.

The parameter "Number of Chip Selects used" should be 1 instead of 2 since only one Chip Select of the processor is being used for both the discrete DRAMs.

Thanks & Regards,
Ritesh M Patel

0 件の賞賛
返信