I am working with the i.MX8ULP processor (MIMX8UD3CVP08SC, revision A2) on my custom PCB. I am working with (effectively) the same DDR as the EVK (MT53E512M32D1ZW-046AUT:B), however I am using the LPDDR4x mode.
I am having trouble with running the NXP IMX DDR Tool, receiving chopped off debug, and hanging at the log pasted below.
[RESULT] Download is complete
Waiting for the target board boot...
===================hardware_init=====================
OCK Set BUCK3 to 0.9v
hardware_init exit
*************************************************************************
*************************************************************************
*************************************************************************
NXP DDR Tool V1.00
Built on Apr 28 2023 11:20:51
*************************************************************************
Waiting for board configuration from PC-end...
The NXP IMX DDR Tool only accommodates for revisions A0 and A1. Is there an updated IMX DDR Tool for the A2 revision?
I have successfully set up my COM communication for the A-Core LPUART7. Does this look right?
memory set 0x298c00bc 32 0x00000443 #PTE15__LPUART7_RX
memory set 0x298c09dc 32 0x00000003 #PTE15__LPUART7_RX
memory set 0x298c00b8 32 0x00000443 #PTE14__LPUART7_TX
memory set 0x298c09e0 32 0x00000003 #PTE14__LPUART7_TX
sysparam set debug_uart 6 #LPUART7 : index from 0 ('0' = UART1, '1' = UART2 and so on)