NXP 1062 MCU Porting http_client_tls_init() example code issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP 1062 MCU Porting http_client_tls_init() example code issue

2,645 Views
jackwu
Contributor I

How do I open the all certificate correctly?

I can only enable this program to open one certificate now, other certificate can't open.

(  Ciphersuite is TLS-ECDHE-ECDSA-WITH-AES-128-GCM-SHA256 )

Can you help provide a way to enable more certificate support through program adjustment and help determine the hardware solution and software solution?

Please help provide a method, thank you!

 

0 Kudos
Reply
5 Replies

2,576 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @jackwu ,

   Thanks for your interest in the NXP MIMXRT product, I would like to provide service for you.

   Please tell me which RT1062 demo you are refering, the SDK verson and the demo path in the SDK package, thanks.

  Then I can help you do the detail checking.

 

Best Regards,

Kerry

0 Kudos
Reply

2,551 Views
jackwu
Contributor I

Hi , @kerryzhou   thanks for your reply , can you provide me your E-mail address ,via email provide you SDK version .

 

Thanks!

Best regards,

Jack 

0 Kudos
Reply

2,545 Views
jackwu
Contributor I

@kerryzhou  NXP 1062 SDK is 2.8.4 version 

 

Thanks .

Best regards,

Jack

0 Kudos
Reply

2,534 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @jackwu ,

   Thanks for your information.

   Your SDK is really very old, please use the newest SDK2.14.0:

https://mcuxpresso.nxp.com/en/builder?hw=EVK-MIMXRT1060

  Whether still have the issues or not?

Please also tell me your used sdk project:

\SDK_2_14_0_EVK-MIMXRT1060\boards\evkmimxrt1060\lwip_examples\lwip_httpssrv_mbedTLS\freertos

This one?

 

Best Regards,

Kerry

 

 

0 Kudos
Reply

2,547 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hello,

   Thanks for your updated information.

  If you want the provide support, you can create the private case, then we can discuss it in the email instead of the public community.

  This is the case create flow:

1. Open below SUPPORT site, click blue "Go to Tickets" in the middle.
http://www.nxp.com/support/support:SUPPORTHOME

2.Then you will be requested to Login, if you have no an account, please first Register with your business email.

3.After login, please "Create New Cases" button in the middle, then you can submit your question.

  In your case content, you can write assign to kerry zhou, and also tell me your SDK version, then I will help you.

Best Regards,

Kerry

0 Kudos
Reply