NVP6324 Format Not Match error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NVP6324 Format Not Match error

2,833件の閲覧回数
FOC
Contributor I

Hi all,

I am experiencing an issue while integrating the NVP6324 video decoder with the i.MX8M Mini SOM. The device is recognized as /dev/video0, but I am encountering a format mismatch error when attempting to stream video through the MIPI-CSI interface. And for mipi driver I'm using mxc_mipi_csi. I've attached my dts and console logs.

I've check this and this 

And here's the modified mxc_mipi_csi.c format section for color formatting:

static const struct csis_pix_format mipi_csis_formats[] = {
{
.code = MEDIA_BUS_FMT_UYVY8_2X8,
.fmt_reg = MIPI_CSIS_ISPCFG_FMT_YCBCR422_8BIT,
.data_alignment = 16,
}, {
.code = MEDIA_BUS_FMT_VYUY8_2X8,
.fmt_reg = MIPI_CSIS_ISPCFG_FMT_YCBCR422_8BIT,
.data_alignment = 16,
}, {
.code = MEDIA_BUS_FMT_SBGGR8_1X8,
.fmt_reg = MIPI_CSIS_ISPCFG_FMT_RAW8,
.data_alignment = 8,
}
};

Can you support me in this issue?

Regards

ラベル(2)
0 件の賞賛
返信
1 返信

2,799件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Make sure that you are playing with the same kernel as the note, should be the 4.14.98.

regards

0 件の賞賛
返信