NVCC_DRAM Operating Ranges when DDR3L

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NVCC_DRAM Operating Ranges when DDR3L

Jump to solution
3,029 Views
ko-hey
Senior Contributor II

Hi all,

I'm using a i.MX6SL.

Let me confirm about DDR3L operating ranges.

What is DDR3L's I/O supply operating ranges ?

There is no description about in Table 9 of datasheet.

Ko-hey

Labels (1)
0 Kudos
Reply
1 Solution
2,863 Views
art
NXP Employee
NXP Employee

DDR3L memories are rated for the operation at 1.35V I/O voltage. Typical I/O voltage range for this type of memory is 1.29V to 1.45V with nominal value of 1.35V. i.MX6SL supports this I/O voltage range.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
4 Replies
2,864 Views
art
NXP Employee
NXP Employee

DDR3L memories are rated for the operation at 1.35V I/O voltage. Typical I/O voltage range for this type of memory is 1.29V to 1.45V with nominal value of 1.35V. i.MX6SL supports this I/O voltage range.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,863 Views
ko-hey
Senior Contributor II

Hi Artur

Let me confirm again.

According to the IMX6SLCEC, NVCC_DRAM support 1.14 V to 1.574 V and DDR3L memory's operating range is 1.29 V to 1.45 V.

So there is no concern about using DDR3L.

Is it correct ?

pastedImage_0.png

Ko-hey

0 Kudos
Reply
2,863 Views
art
NXP Employee
NXP Employee

Yes, this is correct.

Artur

0 Kudos
Reply
2,863 Views
ko-hey
Senior Contributor II

Hi Artur,

Thanks !

Ko-hey

0 Kudos
Reply