NOR Flash partition table for storing Uboot, linux kernel and root file system on IMX6 processor platform

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NOR Flash partition table for storing Uboot, linux kernel and root file system on IMX6 processor platform

1,720件の閲覧回数
SumitVaidya
Contributor II

Hi,

 

Recently I was able to boot IMX6 evaluation board successfully with linux as my OS.

I was browsing through the uboot source code for checking partition for uboot, linux kernel and rootfs on the NOR flash. I downloaded source code for bootloader using 'ltib' command.

 

As per my understanding, NOR flash should be divided into 3 partitions as uboot, kernel and rootfs.

Is there a way to find this partition table along with their load address in linux kernel source code? Also if there is any command to download linux kernel source code using LTIB?

 

Thanks in advance.

 

Regards,

Sumit

タグ(1)
0 件の賞賛
返信
0 返答(返信)