NOR Flash partition table for storing Uboot, linux kernel and root file system on IMX6 processor platform

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NOR Flash partition table for storing Uboot, linux kernel and root file system on IMX6 processor platform

1,707 次查看
SumitVaidya
Contributor II

Hi,

 

Recently I was able to boot IMX6 evaluation board successfully with linux as my OS.

I was browsing through the uboot source code for checking partition for uboot, linux kernel and rootfs on the NOR flash. I downloaded source code for bootloader using 'ltib' command.

 

As per my understanding, NOR flash should be divided into 3 partitions as uboot, kernel and rootfs.

Is there a way to find this partition table along with their load address in linux kernel source code? Also if there is any command to download linux kernel source code using LTIB?

 

Thanks in advance.

 

Regards,

Sumit

标记 (1)
0 项奖励
回复
0 回复数