NNAPI: using a delegate that only supports static-sized tensors with a graph that has dynamic tensor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NNAPI: using a delegate that only supports static-sized tensors with a graph that has dynamic tensor

3,147 次查看
jasonliu1
Contributor I

Hi, 

I started training a fpn-ssd-mobilenetv2 model(which is one of the base models provided by the eIQ software) using custom dataset on the software recently. However, when I converted it into a tflite model and implemented it on a board with NNAPI delegate, it tells me that I'm "attempting to use a delegate that only supports static-sized tensors with a graph that has dynamic-sized tensors" and it failed to apply NNAPI delegate.  

I was just wondering what is the cause of this problem and what should I do to avoid it?

Thanks very much!

标签 (1)
0 项奖励
回复
1 回复

3,107 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello jasonliu1,

One possible reason here is that when you use eIQ software to convert the custom model, you choose MLIR as tflite converter. I will recommend to use TOCO instead and see whether this problem is avoided. Thank you.

 

0 项奖励
回复