NIST STS failure

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NIST STS failure

1,679 Views
tsung-chihwang
Contributor III

We already upgraded Linux kernel from 3.14.38 to 4.1.15_2.0.0 so far.

Then I get 140MB from /dev/hwrng to do the test via NIST STS.

But the test failed on  these two items. (LongestRun and RandomExcursions)

Could you give us some suggestions on this RNG issue?

Below is my parameter setting.

 

Length of bit streams (n)                 1,000,000

Number of bit streams (sample size) (M)   1,073

Block Frequency block length              20,000

Non-Overlapping Templates template length 9

Overlapping Template template length      9

Universal block length (L), number of initialization steps (Q) L=7, Q=1,280

Approximate Entropy block length          8

Serial block length                       16

Linear Complexity block length            1,000

Labels (1)
0 Kudos
Reply
1 Reply

1,551 Views
bpe
NXP Employee
NXP Employee

According to our information, you are already in direct communication with an NXP engineer with respect to this issue. If this is not
correct, or if you are not receiving feedback from that person,
please open a Suport Case:

https://nxpcommunity.force.com/community/

0 Kudos
Reply