NIST Random Number Tast failed on imx6ul

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NIST Random Number Tast failed on imx6ul

1,469 Views
prashan
Contributor I

We are using the imx6ul processor in an application where NIST certification for random number generation sources is required. For this, we capture ~140MB of random data from  /dev/hwrng interface and fead it to the NIST statistical tests. The test parameters used were as follows.

 

./assess 1000000

 

Block Frequency block length        20000

Non-Overlapping Templates template length  9

Overlapping Template template length    9

Approximate Entropy block length      8

Serial block length            16

Linear Complexity block length       1000

 

Number of bit streams (sample size) (M)   1073

 

The minimum size of data  tested is 128mb. So two test samples were created by taking the 1st 128mb and last 128mb of the captured 140mb of data from the processor. According to the final analysis reports, in the last data portion a NonOverlappingTemplate test scores below the minimum pass rate. So we captured several data samples and ran the test. The results are not consistent, some tests passed and some failed.

 

Why does this happen in the /dev/hwrng interface?

What are the implications of this result on the certification?

Is there any specific configuration for the CAAM RNG that we should use? We are using yocto linux-3.14.38 without any modifications.

PS:

imx6ul SRM says the RNG should be instantiated in test mode to obtain data for certification. Even in test mode some tests fail. Below are extracts from the failed test reports for /dev/hwrng:

 

------------------------------------------------------------------------------

 C1  C2  C3  C4  C5  C6  C7  C8  C9 C10  P-VALUE  PROPORTION  STATISTICAL TEST

------------------------------------------------------------------------------

113 111  95 102  91 111  95 109 122 124  0.290066   1051/1073 *  NonOverlappingTemplate

 

------------------------------------------------------------------------------

 C1  C2  C3  C4  C5  C6  C7  C8  C9 C10  P-VALUE  PROPORTION  STATISTICAL TEST

------------------------------------------------------------------------------

109 109  91  94 108 123 112  98 108 121  0.411806   1051/1073 *  NonOverlappingTemplate##

Labels (1)
0 Kudos
Reply
1 Reply

1,094 Views
Yuri
NXP Employee
NXP Employee

Hello,

  the following may be helpful :

https://community.nxp.com/thread/437691 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply