NFS mount rootfs fail from boot but it is work when from the kernel

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NFS mount rootfs fail from boot but it is work when from the kernel

1,292 Views
tomgao
Contributor III

the fail log:

imx mcc test is registered.

input: gpio-keys.21 as /devices/soc0/gpio-keys.21/input/input8

snvs_rtc 20cc034.snvs-rtc-lp: setting system clock to 1970-01-01 00:00:01 UTC (1)

ALSA device list:

  #0: wm8962-audio

  #1: imx-hdmi-soc

random: nonblocking pool is initialized

VFS: Unable to mount root fs via NFS, trying floppy.

VFS: Cannot open root device "nfs" or unknown-block(2,0): error -6

Please append a correct "root=" boot option; here are the available partitions:

1f00              32 mtdblock0  (driver?)

b300         7757824 mmcblk3  driver: mmcblk

  b301          512000 mmcblk3p1 00000000-01

  b302         7143424 mmcblk3p2 00000000-02

b318             128 mmcblk3rpmb  (driver?)

b310            1024 mmcblk3boot1  (driver?)

b308            1024 mmcblk3boot0  (driver?)

Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(2,0)

CPU2: stopping

CPU: 2 PID: 0 Comm: swapper/2 Not tainted 3.14.28-1.0.0_ga+g91cf351 #2

[<800149f8>] (unwind_backtrace) from [<80011714>] (show_stack+0x10/0x14)

[<80011714>] (show_stack) from [<806ecc7c>] (dump_stack+0x7c/0xbc)

[<806ecc7c>] (dump_stack) from [<80013998>] (handle_IPI+0x144/0x158)

[<80013998>] (handle_IPI) from [<80008598>] (gic_handle_irq+0x58/0x5c)

[<80008598>] (gic_handle_irq) from [<80012200>] (__irq_svc+0x40/0x70)

Exception stack(0xa80a9f50 to 0xa80a9f98)

9f40:                                     a80a9f98 3b9aca00 1148b60e 00000017

Labels (2)
0 Kudos
Reply
2 Replies

1,029 Views
tomgao
Contributor III

Now I busy on the other project . could you explain more detail?  I can check after the project .

0 Kudos
Reply

1,029 Views
joanxie
NXP TechSupport
NXP TechSupport

could you share the completed boot log file with me? it seems you set nfs boot incorrectly.

0 Kudos
Reply