NAND boot problem after enable SECURE_BOOT in uboot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NAND boot problem after enable SECURE_BOOT in uboot

1,341件の閲覧回数
SJA
Contributor II

Using IMX6UL EVK with IMX6UL chip in open mode I can boot from NAND without any problem

but only if CONFIG_SECURE_BOOT is not enabled in uboot.

if enable CONFIG_SECURE_BOOT in uboot then booting from NAND no longer works,

I get no output. (Device is in open mode so booting should work even if image is not signed ...)

This same uboot image (with CONFIG_SECURE_BOOT) boots just fine when loaded via USB ...

Have also tried burning the signed uboot image to NAND and still nothing on the output.

ラベル(1)
0 件の賞賛
返信
1 返信

973件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

The following may help.

https://community.nxp.com/thread/380130 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信