NAND Flash and GPIO Boot Overides

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NAND Flash and GPIO Boot Overides

1,027件の閲覧回数
MarkRoy
Contributor III

Hey Folks,

I'm designing a new board based off the QSB.  I am adding two NAND flash chips and connecting them to the EIM_DA[7..0] pins.    These are the same pins used for some of the GPIO boot overides which are sampled at boot when using boot mode 0x00.   If I use 10k pull-ups/downs on these pins to select my desired boot config, will it interfere with normal NAND operation?   Should I instead configure my NAND to use the PATA lines?  Or should I just not use internal boot and boot from fuses instead? 

Suggestions appreciated.

Thanks.

Mark Roy 

タグ(1)
0 件の賞賛
返信
0 返答(返信)