NAND Flash and GPIO Boot Overides

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NAND Flash and GPIO Boot Overides

1,028 Views
MarkRoy
Contributor III

Hey Folks,

I'm designing a new board based off the QSB.  I am adding two NAND flash chips and connecting them to the EIM_DA[7..0] pins.    These are the same pins used for some of the GPIO boot overides which are sampled at boot when using boot mode 0x00.   If I use 10k pull-ups/downs on these pins to select my desired boot config, will it interfere with normal NAND operation?   Should I instead configure my NAND to use the PATA lines?  Or should I just not use internal boot and boot from fuses instead? 

Suggestions appreciated.

Thanks.

Mark Roy 

Tags (1)
0 Kudos
Reply
0 Replies