NAND Flash Has Poor Read Performance

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NAND Flash Has Poor Read Performance

3,225 Views
志林韩
Contributor I

Hello:

   We use NAND Flash : Winbond W29N02GVSIAA, but it has poor read performance.

   I did a simple read performance test:

dd if=/dev/mtdblock3 of=/dev/null bs=512 count=200000

200000+0 records in

200000+0 records out

102400000 bytes (97.7MB) copied, 30.378243 seconds, 3.2MB/s

   Then I found kernel startup log:

      [    0.415944] nand: Unknown W29N02GV

      [    0.415954] nand: 256MiB, SLC, page size: 2048, OOB size: 64  

      [    0.416336] gpmi-nand 112000.gpmi-nand: mode:4 ,failed in set feature.

   So I forced the nand to be in EDO mode 4. Then the read speed reached 10.6MB/s

      dd if=/dev/mtdblock3 of=/dev/null bs=512 count=200000

      200000+0 records in

      200000+0 records out

      102400000 bytes (97.7MB) copied, 9.188045 seconds, 10.6MB/s

   But it's still too slow for us,.

   Thanks for anyone could give me some advice to improve the read performance.

Labels (2)
0 Kudos
Reply
3 Replies

3,012 Views
igorpadykov
NXP Employee
NXP Employee

Hi 志林 韩

for log: nand: Unknown W29N02GV - one can check if this particular part has entry in

linux/drivers/mtd/nand/nand_ids.c

nand_ids.c\nand\mtd\drivers - linux-imx - i.MX Linux kernel 

Also that nand can have many bad blocks so one can try with new one.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,012 Views
志林韩
Contributor I

Hi igorpadykov

Thanks for your reply.

Does it affect its performance if it is not in the list?

0 Kudos
Reply

3,012 Views
志林韩
Contributor I

We use Linux kernel 3.14.52 and UBIFS.

0 Kudos
Reply