NAND Flash Boot Flow and Boot Control Blocks

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NAND Flash Boot Flow and Boot Control Blocks

1,275 Views
takashitakahash
Contributor III

Dear community.

i.MX6DQ RM of  sect 8.5.2.2 NAND Flash Boot Flow and Boot Control Blocks (BCB) Describes

The FCB data structure is protected using software ECC (SEC-DED Hamming Codes).

Do Will ECC data to make the BCH in Software ECC.

Do externally calculated and required to enter ?

The ECC data is recorded in the 0-3 byte of FCB?

Labels (2)
0 Kudos
Reply
1 Reply

1,162 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

FCB data is protected by software ECC, calculated

by arm core, each data byte is protected with parity data.

kobs-ng tool is used for writing FCB data to NAND.


Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------