NAND Flash Boot Flow and Boot Control Blocks

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NAND Flash Boot Flow and Boot Control Blocks

1,303件の閲覧回数
takashitakahash
Contributor III

Dear community.

i.MX6DQ RM of  sect 8.5.2.2 NAND Flash Boot Flow and Boot Control Blocks (BCB) Describes

The FCB data structure is protected using software ECC (SEC-DED Hamming Codes).

Do Will ECC data to make the BCH in Software ECC.

Do externally calculated and required to enter ?

The ECC data is recorded in the 0-3 byte of FCB?

ラベル(2)
0 件の賞賛
返信
1 返信

1,190件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

FCB data is protected by software ECC, calculated

by arm core, each data byte is protected with parity data.

kobs-ng tool is used for writing FCB data to NAND.


Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------