NAND FLASH Boot Flow

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,837件の閲覧回数
takashitakahash
Contributor III

i.MX6 RM described as.8.5.2.2 NAND Flash Boot Flow and Boot Control Blocks (BCB)

Driver reads raw 2112 bytes of first SECTOR and runs through software ECC engine that determines whether FCB data is valid or not.

Please tell me the definition of the Sector in this context.

Is this the first page in the NAND flash Block  (address is smallest)?

ラベル(2)
0 件の賞賛
返信
1 解決策
1,624件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

>Please tell me the definition of the Sector in this context.

>Is this the first page in the NAND flash Block  (address is smallest)?

Yes this is correct understanding. In particular sect.8.5.2.7.1 BCH ECC Page

Organization IMX6DQRM states

The first data block is called block 0 and the rest of the blocks are called block N.

Separate ECC level scan be used for block 0 and block N.

The metadata bytes should be located at the beginning of a page, starting at byte 0..

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,625件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

>Please tell me the definition of the Sector in this context.

>Is this the first page in the NAND flash Block  (address is smallest)?

Yes this is correct understanding. In particular sect.8.5.2.7.1 BCH ECC Page

Organization IMX6DQRM states

The first data block is called block 0 and the rest of the blocks are called block N.

Separate ECC level scan be used for block 0 and block N.

The metadata bytes should be located at the beginning of a page, starting at byte 0..

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信