Mx53 I2C slave patch

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Mx53 I2C slave patch

1,270 次查看
shaojun_wang
NXP Employee
NXP Employee

Hardware connection

In mx53 SMD, connect R85 to R138, connect R86 to R139.

 

mx53_i2c_slave.patch is the patch to support I2C slave in Mx53 SMD, it can be applied to R10.3.2 and 1109.

I2C2 is master, I2C3 is slave.

In menuconfig, select Device Drivers  ---> [*] I2C Slave support

 

mxc_i2c_slave_test.c is the test code, it can be built by below command

/opt/freescale/usr/local/gcc-4.4.4-glibc-2.11.1-multilib-1.0/arm-fsl-linux-gnueabi/bin/arm-none-linux-gnueabi-gcc -lpthread mxc_i2c_slave_test.c -o mxc_i2c_slave_test

 

If the test fail, please check if I2C2_SCL, I2C2_SDA, I2C3_SCL, I2C3_SDA are pulled up to 3.3V, they may be pulled down by the original I2C3 slave device in the board.

Original Attachment has been moved to: mx53_i2c_slave.patch.zip

Original Attachment has been moved to: mxc_i2c_slave_test.c.zip

标签 (3)
0 项奖励
回复
0 回复数