Multiplexed Address/Data Mode access timing for i.MX6DL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Multiplexed Address/Data Mode access timing for i.MX6DL

1,740 次查看
yuuki
Senior Contributor II

Dear all,

We want to use Multiplexed Address/Data mode of EIM of i.MX6DL.
Because EIM_D[15:0] is used as other functions, we use only EIM_DA[15:0] as Address and Data signal of EIM.

We want to check connection and a timing of Multiplexed Address/Data Mode.
However, these contents are not explained in Reference Manual.

May I have a document explaining connection and a timing of Multiplexed Address/Data Mode?

Best Regards,
Yuuki

标签 (1)
0 项奖励
回复
1 回复

1,573 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Please use i.MX 6DL Datasheet. Section 4.9.3 [External Interface Module (EIM)]

of the linked below document, provides EIM hardware specs. In particular,
Table 41 (EIM Internal Module Multiplexing)  shows connections. Timings may be found

on Figure 17 [Muxed Address/Data (A/D) Mode, Synchronous Write Access, WSC=6,ADVA=0, ADVN=1,

and ADH=1] and Figure 18 [16-Bit Muxed A/D Mode, Synchronous Read Access, WSC=7, RADVN=1,

ADH=1, OEA=0]. 

https://www.nxp.com/docs/en/data-sheet/IMX6SDLCEC.pdf 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复