Multiple endpoints using RPMsg RTOS Layer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multiple endpoints using RPMsg RTOS Layer

4,045 Views
rlumo
Contributor II

Does the RPMsg RTOS Layer's create endpoint (rpmsg_rtos_create_ept) supports multiple endpoints?

0 Kudos
Reply
2 Replies

3,917 Views
igorpadykov
NXP Employee
NXP Employee

Hi Roger

>Does the RPMsg RTOS Layer's create endpoint (rpmsg_rtos_create_ept) supports multiple endpoints?

no. Sorry NXP i.MX releases do not support multiple endpoints.

For multiple endpoints example one can look at

Asymmetric Multiprocessing: RPMsg – Linux/Android | Kynetics 

Asymmetric Multiprocessing - Boundary Devices Nitrogen7 | Kynetics 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,798 Views
enricorocheti_
Contributor III

Hello @igorpadykov, RPMsg in the NXP SDK (I'm using the RT1160EVK) still don't support multiple endpoints? 

I was thinking about creating two endpoints in my cores, one channel to send/recv synchronous messages and the other to send/recv asynchronous messages.

Thank you,

Enrico

0 Kudos
Reply