Multiple U-Boot Partitions Possible ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multiple U-Boot Partitions Possible ?

4,699 Views
om26er
Contributor I

I am trying to implement A/B partition scheme for OTA updates. The partition structure could look like this:

1. uboot partition 1

2. uboot partition 2

3 rootfs 1 (includes kernel and dtb)

4 rootfs 2 (includes kernel and dtb)

I am trying to understand how does the i.MX 8MM "knows" where to load the bootloader from ? Is there a way to tell the firmware to load the bootloader (u-boot) from a different partition ? 

I could go with a simpler approach where I have one u-boot partition and two rootfs. However this comes with a risk of breakage if an OTA update of the u-boot partition goes bad due to some reason. Hence I was wondering if it's possible to have bootloader redundancy in the iMX platform ? 

Labels (1)
0 Kudos
Reply
2 Replies

4,695 Views
om26er
Contributor I

Instead of two different partitions for u-boot, I guess if there was a way to keep two copies of u-boot in that partition and for the firmware to somehow have a way to decide which one to load.

something similar to how the Raspberry Pi recently introduced tryboot.txt option.

Of course in the absence of such a possibility the only way would be to never update u-boot over OTA. However that doesn't really sound like a "good" approach IMO. How would we patch any u-boot CVEs then or bug in the bootloader ?

0 Kudos
Reply

4,680 Views
igorpadykov
NXP Employee
NXP Employee

Hi Omer

 

>I am trying to understand how does the i.MX 8MM "knows" where to load the bootloader from ?

 

one can look at Table 1. Image layout, Table 53. Board-specific default values   i.MX Linux User’s Guide​

some addresses (like loadaddr) can be found in

https://source.codeaurora.org/external/imx/uboot-imx/tree/include/configs/imx8mm_evk.h?h=lf_v2021.04

 

Best regards
igor

0 Kudos
Reply