Multiple SDRAM chip support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multiple SDRAM chip support

1,929件の閲覧回数
paulnichols
Contributor I

Can multiple SDRAM chips be added to the RT1050 (eg: MIMXRT1051DVL6A) external memory interface to expand the amount of addressable RAM? For my application I am needing at least 64MB of RAM and to make this cost effective is seems 2 x 32MB (16MB x 16 bit width) chips would be best.

From the datasheet it seems possible using multiple CS line but the following statement from a supporting RT1050 introduction slide deck (page 17 - https://www.nxp.com/docs/en/supporting-information/i.MX-RT1050-Supporting-Inf.pdf) seems to indicate support for only a single 16 bit width DRAM is possible.

"Support single x16 DRAM chip or dual x8 DRAM chip" 

Just needing to confirm I can achieve 64MB (or even 96MB) of extern SDRAM on this platform. 

Thanks

タグ(2)
0 件の賞賛
返信
1 返信

1,728件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

  According to i.MX RT1050 Reference Manual its memory controller SEMC supports

SDRAM interface with the following features:

• 8/16 bit modes;

• Up to 512Mb per each Chip Select (CS) and up to 4 CS.

 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信