Multi core communication between Cortex-A9 and M4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multi core communication between Cortex-A9 and M4

1,849件の閲覧回数
anilchowdary
Contributor II

I have my own evm board with MCIMX6X4EVM10AB processor, I want to check the communication between two cores Cortex-A9 and Cortex-M4 with example. I know it will work with mcc apis. please provide working example.

My setup:

Processor  : MCIMX6X4EVM10AB

toolchain : arm-poky-linux-gnueabi-gcc/g++

Linux Version  : 4.1.15

Thanks for your reply.

thanks & Regards

-Anil

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,624件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi Anil,

Please take a look to the following document Running RPMsg Demo Applications for Multicore Communication with IMX6SX and IMX7D 


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,624件の閲覧回数
anilchowdary
Contributor II

Thanks Carlos_Musich it helps a lot

0 件の賞賛
返信