Multi core communication between Cortex-A9 and M4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi core communication between Cortex-A9 and M4

1,850 Views
anilchowdary
Contributor II

I have my own evm board with MCIMX6X4EVM10AB processor, I want to check the communication between two cores Cortex-A9 and Cortex-M4 with example. I know it will work with mcc apis. please provide working example.

My setup:

Processor  : MCIMX6X4EVM10AB

toolchain : arm-poky-linux-gnueabi-gcc/g++

Linux Version  : 4.1.15

Thanks for your reply.

thanks & Regards

-Anil

Labels (1)
0 Kudos
Reply
2 Replies

1,625 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Anil,

Please take a look to the following document Running RPMsg Demo Applications for Multicore Communication with IMX6SX and IMX7D 


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,625 Views
anilchowdary
Contributor II

Thanks Carlos_Musich it helps a lot

0 Kudos
Reply