Multi Touch Issue in Android 7.1.1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multi Touch Issue in Android 7.1.1

1,681件の閲覧回数
rizwanm
Contributor II

HI,

Am facing multi touch problem with IMX6 Dual lite board in android 7.1.1.

we are configuring touch in i2C3 Size 7inch 700X480

LCD Actron Touch with  Driver HY463X

if configure as a multi touch it is not working

XY Coordinates  are changing >>
i also observed some below error in  logcat | grep -nir "InputReader"

(standard input):475:01-01 00:00:29.696   484   516 I InputReader:   Touch device 'hy46xx_ts' could not query the properties of its associated display.  The device will.
(standard input):476:01-01 00:00:29.696   484   516 I InputReader: Device added: id=1, name='hy46xx_ts', sources=0x00001002
(standard input):483:01-01 00:00:29.761   484   516 I InputReader: Reconfiguring input devices.  changes=0x00000004
(standard input):484:01-01 00:00:29.761   484   516 I InputReader: Device reconfigured: id=1, name='hy46xx_ts', size 800x48

Please help to resolve this problem

Best Regards,

Rizwan M

ラベル(1)
0 件の賞賛
返信
1 返信

1,437件の閲覧回数
rizwanm
Contributor II

Add IDC file in below directory with XY Orientation 

Create idc file along with your touch driver name ie hy46xx_ts.idc

file contant should be

touch.deviceType = touchScreen
touch.orientationAware = 1

touch.size.calibration = none
touch.orientation.calibration = none

Place the idc file in system/usr/idc/

Hopefully it works!

Warm Regards,

Rizwan M

0 件の賞賛
返信