Motor control using Imx8mm

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Motor control using Imx8mm

1,835 Views
hsiddiquee
Contributor II

Hello,

Our company is using imx8mm to make a device. There are bunch of processes going on in the imx processor. Like image processing, multiple motors (Mostly at different time), display, etc. For two specific motor control, we need to keep changing it's angle to specific degrees. One motor angle is track by potentiometer (may need ADC). 

Can you guys suggest, if we should use separate 8bit micro-controller for motor control or should we control it directly from imx8mm. 

 

Thank you

Labels (1)
0 Kudos
Reply
2 Replies

1,827 Views
igorpadykov
NXP Employee
NXP Employee

Hi hsiddiquee

 

unfortunately i.MX8M Mini has not adc, for motor applications may be useful

GPT1 capture capability (measure phase difference between input signals),

example can be found in M4 SDK_EVK-MIMX8MM (..driver_examples/gpt/capture/ folder)

available on https://mcuxpresso.nxp.com/en/welcome

 

Best regards
igor

0 Kudos
Reply

1,433 Views
MPUUser
Contributor I

Hi,

 

Does iMX8MPLus also has this function?

GPT1 capture capability (measure phase difference between input signals).

 

How many independent input capture can the 8MPlus support?

I have 4 motors with optical encoder feedback. They can be single phase or 2 phase.

Can it support 4 x single phase? Or better still, 4 x 2 phase encoder inputs?

 

Thanks.

0 Kudos
Reply