Motor Control Software on RT1064

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Motor Control Software on RT1064

2,367件の閲覧回数
Carlio
Contributor II

Hi there,

When I’m trying to create my SDK in MCUExpresso SDK Builder, the “Motor Control Software” is not available as an option. However, it is supported for the RT1062. Are there any differences between the two processors here that I have missed? Is the Motor Control Software not supported for RT1064, and in that case why?

0 件の賞賛
返信
3 返答(返信)

2,327件の閲覧回数
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @Carlio,

Meanwhile, you can use any of the motor control examples found in the SDK for the RT1060 in the RT1064.

0 件の賞賛
返信

2,319件の閲覧回数
Carlio
Contributor II

Thank you @Alexis_A ! Will do. 

0 件の賞賛
返信

2,346件の閲覧回数
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @Carlio,

I also think that this middleware should be able for both MCUs, let me check internally if there's a reason that this software is missing.

Best Regards,

Alexis Andalon