Motor Control Software on RT1064

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Motor Control Software on RT1064

2,402 Views
Carlio
Contributor II

Hi there,

When I’m trying to create my SDK in MCUExpresso SDK Builder, the “Motor Control Software” is not available as an option. However, it is supported for the RT1062. Are there any differences between the two processors here that I have missed? Is the Motor Control Software not supported for RT1064, and in that case why?

0 Kudos
Reply
3 Replies

2,362 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @Carlio,

Meanwhile, you can use any of the motor control examples found in the SDK for the RT1060 in the RT1064.

0 Kudos
Reply

2,354 Views
Carlio
Contributor II

Thank you @Alexis_A ! Will do. 

0 Kudos
Reply

2,381 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @Carlio,

I also think that this middleware should be able for both MCUs, let me check internally if there's a reason that this software is missing.

Best Regards,

Alexis Andalon