More than 4 CS lines for SPI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

More than 4 CS lines for SPI

Jump to solution
1,289 Views
marcus_cps
Contributor I

The documentation for iMX6UL and iMX8 says SPI has 4 CS lines.


I intend to use a total of 12 SPI devices connected to SPI1, 2 and 3 (4 in each).
As far as I understood, I can configure CS pins as GPIO and use the kernel driver configurations to define all 12 CS lines from GPIOs.

Is my understanding correct or is there some hardware limitation I'm missing?

Thanks

1 Solution
1,241 Views
igorpadykov
NXP Employee
NXP Employee

Hi Marcus

yes this understanding is correct.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
1,242 Views
igorpadykov
NXP Employee
NXP Employee

Hi Marcus

yes this understanding is correct.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------