Modify LED brightness level

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Modify LED brightness level

2,340 Views
pehenazam
Contributor I

I'd to modify minimum/maximum brightness for the LED driver (PCA9632 driver). in linux I have the interface for to set brightness level between 0 and 10 using interface `/sys/class/backlight/backlight_keypad/`

I can modify `/sys/class/backlight/backlight_keypad/brightness` but I cannot modify it out of 0-10. I like to have it 0-256 so I can have lower brightness. Based on the driver datasheet  and driver source in Individual brightness control mode, each LED output has its own 8-bit resolution (256 steps) so it should be possible to set 0-256. But where should I change it so I would have all 0-256 levels, in the driver source code or linux kernel or somewhere else?

Thanks

Labels (2)
0 Kudos
Reply
1 Reply

2,143 Views
igorpadykov
NXP Employee
NXP Employee

Hi Pehen

one can check what actual values are written by driver/application, as brightness change

may be very small for 1 bit and it intentionally uses less levels. For debugging one can use

AN4553 Using Open Source Debugging Tools for Linux on i.MX Processors
http://www.nxp.com/assets/documents/data/en/application-notes/AN4553.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply