Model tensorflow 1 can't run on NPU iMX8MP and fallback to CPU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Model tensorflow 1 can't run on NPU iMX8MP and fallback to CPU

515 Views
The_Nguyen
Contributor I

Hi, NXP supporter,

I'm tried running model mobilenet-v1 with tensorflow 1.15 and quantized with eIQ-tool. However, when I run on NPU it gets fallback error to CPU but still recognizes the object and I want it to run on NPU. I tried with exporting tflite_graph.pb to saved_model and quantization with tensorflow 2.16.2 environment. I used the following method to quant but it still doesn't work, how can I run it completely on NPU without falling back to CPU for processing. 

def representative_data_gen():
  dataset_list = quant_image_list
  quant_num = 500
  for i in range(quant_num
    pick_me = random.choice(dataset_list)
    image = tf.io.read_file(pick_me)

    if pick_me.endswith('.png') or pick_me.endswith('.PNG'
      image = tf.io.decode_jpeg(image, channels=3)
    image = tf.image.resize(image, [width, height])
    image = tf.cast(image / 255., tf.float32)
    image = tf.expand_dims(image, 0)
    yield [image]
converter = tf.lite.TFLiteConverter.from_saved_model(saved_model)

converter.optimizations = [tf.lite.Optimize.DEFAULT]
converter.representative_dataset = representative_data_gen
converter.target_spec.supported_ops = [tf.lite.OpsSet.TFLITE_BUILTINS_INT8]
converter.target_spec.supported_types = [tf.int8]
converter.inference_input_type = tf.int8
converter.inference_output_type = tf.int8  
tflite_model = converter.convert() 
Below is my email and I need help with this issue: the.nguyen@rynantech.com
0 Kudos
Reply
2 Replies

490 Views
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @The_Nguyen 

I hope you are doing very well.

 

Please refer to chapter 2.7.1 Running the example on the i.MX 8 platform hardware accelerator of i.MX Machine Learning User's Guide.

There is described how you can run a mobilnet with hardware acceleration GPU/NPU.

 

Best regards,

Salas.

0 Kudos
Reply

475 Views
The_Nguyen
Contributor I

Hello Salas, 

I followed the instructions in the document in 2.7.1, I was able to run the example model, but for the mobilenet-v1 model, I quantized it with eIQ-tool and it could not run completely on the NPU. So the reason is that the model has not been fully quantized to int8 or is my configuration incorrect.

I read in the document that in iMX8MP, it is required to be fully quantized to int8 to be able to run completely on the NPU without falling back to the CPU, is that correct?

Thanks and Regards,

TheNguyen

0 Kudos
Reply