Mix configuration on imx8m android9

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Mix configuration on imx8m android9

2,294 次查看
raman_thapar
Contributor II

I am using a CX20921 codec with an IMX8m mini and have the driver working to the point I see the device under /dev/sound. I can record audio using tinycap under Linux. 

However I don't see the mic in Android.  How do I hook the mic up into Android? Any pointers will be helpful.

Thanks!

0 项奖励
回复
3 回复数

2,157 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Raman

one can look at android resources:

Android: How to configure "tinymix" to record system audio with "tinycap" - Stack Overflow 

http://www.programmersought.com/article/9586201076/ 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,157 次查看
raman_thapar
Contributor II

Thanks Igor. The links seem to be more about getting tinycap to work. For me tinycap is working and I am able to record and playback the recording in Linux.

I am wondering if there is anything I need to do so Android is able to use the mic. For example configuring audio configuration xml files or any other settings to let Android know about the connected device.

My mic is connected to the system via a codec and is using I2s as the input source for data.

Thanks!

0 项奖励
回复

2,157 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Raman

also one can look at Android for Nitrogen8M Mini (it has wm8960 codec)

https://boundarydevices.com/wiki/android-for-nitrogen8/ 

Best regards
igor

0 项奖励
回复