Missing /dev/galcore in Linux kernel 4.14.x

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Missing /dev/galcore in Linux kernel 4.14.x

3,132件の閲覧回数
henrik1
Contributor I

Using the 4.14 Linux kernel from GitHub - Freescale/linux-fslc at 4.14.x+fslc I get the following issue

open("/dev/galcore", O_RDWR) = -1 ENOENT (No such file or directory)
open("/dev/graphics/galcore", O_RDWR) = -1 ENOENT (No such file or directory)

A little digging about suggests that this is related to the mxc driver present in the latest BSP from NXP which is for 4.9.  When is the BSP for Linux kernel 4.14 expected to be released?

0 件の賞賛
返信
2 返答(返信)

2,599件の閲覧回数
henrik1
Contributor I

Hi,

We are using the 4.1.15 BSP you have released for now, but require drivers that were introduced much later.  Backporting the drivers is simply not feasible unfortunately.  When is the BSP for Linux Kernel 4.14 expected to be released?

0 件の賞賛
返信

2,599件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Henrik,

     We released 3 versions of BSP for Linux 4.x: 4.1.15 & 4.9.x(11&51). So please use linux BSP that we formally released.

Have a nice day!

TIC Weidong Sun

0 件の賞賛
返信