HDMI connectivity on i.MX8M

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HDMI connectivity on i.MX8M

552 Views
ilko
Contributor I

Hi,
According to i.MX 8MDQLQ Hardware Developer’s Guide the HDMI signals should be connected to the HDMI connector through RC groups (100nF, 604R).
In case that the distance between CPU and connector is long, how should be placed the RC group?
The capacitor close to the CPU and the resistor close to the connector?

Regards,
Ilko Iliev

0 Kudos
2 Replies

413 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ilko 

both capacitor and the resistor should be placed close to the CPU.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

413 Views
ilko
Contributor I

Thank you!

0 Kudos