Hi all
Let me confirm about the reset value in i.MX27.
I read chapter 3 of MCIMX27 Multimedia Applications Processor Reference Manual (MCIMX27RM Rev. 0.4 06/2012).
Q1
0x1002_700C (SPCTL0) SPLL Control Register 0
The reset value of Table 3-4 and Figure 3-7 doesn't match. Which is correct ?
Q2
0x1002_7018 (PCDR0) Peripheral Clock Divider Register 0
The reset value of Table 3-4 and Figure 3-10 doesn't match. Which is correct ?
Q3
0x1002_701C (PCDR1) Peripheral Clock Divider Register 1
The reset value of Table 3-4 and Figure 3-11 doesn't match. Which is correct ?
Ko-hey