Mismatch of Output Buffer Impedance and Drive Strength Field

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Mismatch of Output Buffer Impedance and Drive Strength Field

Jump to solution
1,398 Views
ko-hey
Senior Contributor II

Hi all

Let me confirm Output Buffer Impedance and Drive Strength Field with i.MX6UL.

I think there are some wrong description about Output Buffer Impedance and Drive Strength Field.

I'm refering the following documents.
IMX6ULCEC Rev. 1, 04/2016
IMX6ULRM Rev. 1, 04/2016

Here is a table which shows the relationship between Output Buffer Impedance and DSE in IMX6ULCEC.

pastedImage_1.png

On the other hand, here is a table which shows the setting of DSE and the impedance value in IMX6ULRM.

pastedImage_2.png

Comparing the above, I think the table 33 of IMX6ULCEC is for OVDD = 3.3V and table 34 is for OVDD = 1.8V.

Am I correct ?

Ko-hey

Labels (1)
0 Kudos
Reply
1 Solution
1,269 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Ko-hey,

Thanks for pointing this out! What seems to be switched is the Drive Strength Field on the pad register impedances and voltages. The Datasheet tables look correct.

I’ll forward this error to the documentation team so it gets addressed on future releases of the documentation.

Regards,

View solution in original post

0 Kudos
Reply
2 Replies
1,270 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Ko-hey,

Thanks for pointing this out! What seems to be switched is the Drive Strength Field on the pad register impedances and voltages. The Datasheet tables look correct.

I’ll forward this error to the documentation team so it gets addressed on future releases of the documentation.

Regards,

0 Kudos
Reply
1,268 Views
ko-hey
Senior Contributor II

Hello gusarambula

Thank you for reply.

I understand.

Ko-hey

0 Kudos
Reply