Mircast source support with Android BSP REV L5.0.0 on sabresd

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Mircast source support with Android BSP REV L5.0.0 on sabresd

3,814 Views
rameshbabup
NXP Employee
NXP Employee

Hello,

Please let me know the availability of Miracast source support for Android BSP REV L5.0.0 on sabresd.

When checked display settings, it has only "Cast screen", not Wi-Fi display.

Any info on this will be appreciated.

Thanks,

Ramesh

Labels (4)
0 Kudos
Reply
3 Replies

3,575 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ramesh

below part of Android_Release_Notes.pdf document

included in Android L5 package

1.jpg

2.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,575 Views
rameshbabup
NXP Employee
NXP Employee

Hi Igor,

Thanks, I had checked that and it was mentioned about Wi-Fi Display Sink, not the "Source".

Booted Android bsp on Sabresd and was able to get Sink working using wfdsink app.

But "Cast Screen" from Display settings does not work.

Wanted to know if there is a way enable Wi-Fi Display Source / Miracast Source.

My understanding is that Cast Screen does not use Wi-Fi Display, its rather Android's way of doing Miracast. Is that right?

Please comment.

Thanks,

Ramesh

0 Kudos
Reply

3,575 Views
XiaoPong
NXP Employee
NXP Employee

wfdsink app is located at myandroid/device/wfd-proprietary

Miracast source is located at myandroid/frameworks/av/media/libstagefright/wifi-display/source

0 Kudos
Reply