Mircast source support with Android BSP REV L5.0.0 on sabresd

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Mircast source support with Android BSP REV L5.0.0 on sabresd

3,818件の閲覧回数
rameshbabup
NXP Employee
NXP Employee

Hello,

Please let me know the availability of Miracast source support for Android BSP REV L5.0.0 on sabresd.

When checked display settings, it has only "Cast screen", not Wi-Fi display.

Any info on this will be appreciated.

Thanks,

Ramesh

ラベル(4)
0 件の賞賛
返信
3 返答(返信)

3,579件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ramesh

below part of Android_Release_Notes.pdf document

included in Android L5 package

1.jpg

2.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,579件の閲覧回数
rameshbabup
NXP Employee
NXP Employee

Hi Igor,

Thanks, I had checked that and it was mentioned about Wi-Fi Display Sink, not the "Source".

Booted Android bsp on Sabresd and was able to get Sink working using wfdsink app.

But "Cast Screen" from Display settings does not work.

Wanted to know if there is a way enable Wi-Fi Display Source / Miracast Source.

My understanding is that Cast Screen does not use Wi-Fi Display, its rather Android's way of doing Miracast. Is that right?

Please comment.

Thanks,

Ramesh

0 件の賞賛
返信

3,579件の閲覧回数
XiaoPong
NXP Employee
NXP Employee

wfdsink app is located at myandroid/device/wfd-proprietary

Miracast source is located at myandroid/frameworks/av/media/libstagefright/wifi-display/source

0 件の賞賛
返信