Minimum external DDR3 amount

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Minimum external DDR3 amount

2,080 Views
olli_mannisto
Contributor II

The i.MX7Solo datasheet says the DDR interface density is 256MB to 2GB (9.1.2 table 9-1). Does that actually mean that using 512Mbit or 1Gbit DDR3 chips is out of the question?

Labels (1)
0 Kudos
Reply
2 Replies

1,994 Views
Yuri
NXP Employee
NXP Employee

Hello,

   i.MX7 DDRC supports devices with column size of 8-12 bits and row size of 11-16 bits;

data port size 16/32-bit; up to two CSs. Total memory size is restricted by 2048 MBytes (look at system

memory map).


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,994 Views
olli_mannisto
Contributor II

Hei, 

I was asking about minimum memory size. Are we fine with 512Mbit (32MBx16) part that's organized 12bit Row, 10bit Column? Apparently yes, but the datasheet claims 256MB is the minimum RAM size? 

0 Kudos
Reply