Minicom Package - Not Installed

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Minicom Package - Not Installed

2,735 次查看
PaulDeMetrotion
Senior Contributor I

I built a new kernel with LTIB and selected the minicom and lszrz packages. Build completed and I can confirm that the Mincom package was built. Problem is now that I have booted into the kernel, I get the following message:

     The program 'minicom' is currently not installed.  You can install it by typing: apt-get install minicom

Obviously I can install from the command line as they suggested, but why isn't it already there? Is there another step I have missed?

0 项奖励
回复
5 回复数

2,541 次查看
PaulDeMetrotion
Senior Contributor I

No my target rootfs is the Freescale Ubuntu version 4.0.0. I do not want to copy the LTIB rootfs. I guess I will try the second option. Do I need to do the same thing for any other packages I decide to include?

0 项奖励
回复

2,541 次查看
LeonardoSandova
Specialist I

Oh I see. I think you better use apt-get system to install stuff on Ubuntu. Copying binaries from LTIB rootfs  to Ubuntu is not safe and apps may not work.

Leo

0 项奖励
回复

2,541 次查看
PaulDeMetrotion
Senior Contributor I

There is nothing. I noticed that in my built rootfs directory there is a /usr/bin/minicom file. Do I need to copy this to my target media as well as the uImage?

0 项奖励
回复

2,541 次查看
LeonardoSandova
Specialist I

so, your ltib/rootfs is not the same as the target rootfs. You can either flash your SD with the ltib's rootfs or try just copying minicom bin into target. This last option works if all run-time libraries are already installed on your target.

Leo

0 项奖励
回复

2,541 次查看
LeonardoSandova
Specialist I

Try to do a global find minicom ('find / | grep minicom') and see if that path where it resides is in your PATH environment variable.

0 项奖励
回复