Micro-Processor for DAC And ADC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Micro-Processor for DAC And ADC

2,386件の閲覧回数
ashokb
Contributor I

Hi All,

We are Designing ultrasound device for that we are using dual channel, high voltage Transmitter(TX517) and DAC(ADS4128).

can anyone suggest me a  IMX 6 or any other micro- processor  part number suitable both interface.

Below attached the our application block diagram.

Thanks,

Ashok

ラベル(5)
0 件の賞賛
返信
1 返信

2,307件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi Ashok,

In case of the ultrasound transmitter, if it uses GPIOs as interface, practically any i.MX processor could be used to drive it (or actually any other microcontroller).

However, in case of the high-speed ADC, its datasheet mentions that has LVDS output, and I’m afraid that we don’t have any processor/controller with LVDS input; the parts with LVDS module could be only used as output, so, you may consider a different ADC with other compatible high-speed interface.

Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

0 件の賞賛
返信