Micro-Processor for DAC And ADC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Micro-Processor for DAC And ADC

2,369 Views
ashokb
Contributor I

Hi All,

We are Designing ultrasound device for that we are using dual channel, high voltage Transmitter(TX517) and DAC(ADS4128).

can anyone suggest me a  IMX 6 or any other micro- processor  part number suitable both interface.

Below attached the our application block diagram.

Thanks,

Ashok

Labels (5)
0 Kudos
Reply
1 Reply

2,290 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Ashok,

In case of the ultrasound transmitter, if it uses GPIOs as interface, practically any i.MX processor could be used to drive it (or actually any other microcontroller).

However, in case of the high-speed ADC, its datasheet mentions that has LVDS output, and I’m afraid that we don’t have any processor/controller with LVDS input; the parts with LVDS module could be only used as output, so, you may consider a different ADC with other compatible high-speed interface.

Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

0 Kudos
Reply