Mfgtool2 tool not working

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Mfgtool2 tool not working

1,635件の閲覧回数
logifrancis
Contributor III

Hi,

I have designed a board with iMX6 processor. It is powered up and basic testing is done. I am trying to using Mfgtool2 to download my uboot image to  SD card. . I have powered the board an connected the OTG USB port to PC. After that i have opened the Mfgtool2 application. But when i open the tool it is not working The error i am getting is given below. (error code:4). I am also attachint the log file for the details. Can anyone help on this?

pastedImage_1.png

0 件の賞賛
返信
1 返信

1,454件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

what mfgtool version and board you use? when you connect board to PC, can mfgtool recognize the board? if yes, pls dont insert the SD card first, when mfgtool recognize the board, then insert the SD card.

0 件の賞賛
返信