Mfgtool download imx6ql eMMC error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Mfgtool download imx6ql eMMC error

2,966件の閲覧回数
yenchou
Contributor III

Freescale board:MX6-SabreSD

Demo image: android_M6.0.1_2.1.0_image_6dqpsabresd

I used u-boot command to erase emmc.

=> mmc list
FSL_SDHC: 0
FSL_SDHC: 1 (SD)
FSL_SDHC: 2 (eMMC)

=> mmc dev 2
switch to partitions #0, OK
mmc2(part 0) is current device

=> mmc read ${loadaddr} 0x7fffffff 1

MMC read: dev # 2, block # 2147483647, count 1 ... MMC: block number 0x80000000 exceeds max(0xecc000)
0 blocks read: ERROR

=> mmc erase 0 0xecc000

MMC erase: dev # 2, block # 0, count 15515648 ... 15515648 blocks erased: OK

Then I repeated the behavior in dev 2 1,dev 2 2 and dev 2 3.

Finally,burn demo image into emmc.

Before the problem occured,I allready have burned demo image into emmc and  worked normally in serveral times .

The error ocured and produced log.

U-Boot 2015.04-imx_v2015.04_4.1.15_1.0.0_ga+g384e1c1 (Mar 13 2016 - 17:31:03)

CPU: Freescale i.MX6Q rev1.2 at 792 MHz
CPU: Temperature 32 C
Reset cause: POR
Board: MX6-SabreSD
I2C: ready
DRAM: 1 GiB
PMIC: PFUZE100 ID=0x10
MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
*** Warning - bad CRC, using default environment

No panel detected: default to Hannstar-XGA
Display: Hannstar-XGA (1024x768)
In: serial
Out: serial
Err: serial
switch to partitions #0, OK
mmc1 is current device
Net: FEC [PRIME]
Boot from USB for mfgtools
Use default environment for mfgtools
Run bootcmd_mfg: run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};
Hit any key to stop autoboot: 0
Kernel image @ 0x12000000 [ 0x000000 - 0x552a48 ]
## Loading init Ramdisk from Legacy Image at 12c00000 ...
Image Name: fsl-image-mfgtool-initramfs-imx6
Image Type: ARM Linux RAMDisk Image (gzip compressed)
Data Size: 7565864 Bytes = 7.2 MiB
Load Address: 00000000
Entry Point: 00000000
Verifying Checksum ... OK
## Flattened Device Tree blob at 18000000
Booting using the fdt blob at 0x18000000
Using Device Tree in place at 18000000, end 1800e197
switch to ldo_bypass mode!

Starting kernel ...

Booting Linux on physical CPU 0x0
Linux version 4.1.15-1.0.0-mfgtool+g3924425 (bamboo@shlinux12) (gcc version 5.2.0 (GCC) ) #1 SMP PREEMPT Sun Mar 13 17:19:17 CST 2016
CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c5387d
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine model: Freescale i.MX6 Quad SABRE Smart Device Board
Reserved memory: created CMA memory pool at 0x3c000000, size 320 MiB
Reserved memory: initialized node linux,cma, compatible id shared-dma-pool
Memory policy: Data cache writealloc
PERCPU: Embedded 12 pages/cpu @ab705000 s16768 r8192 d24192 u49152
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 260096
Kernel command line: console=ttymxc0,115200 rdinit=/linuxrc g_mass_storage.stall=0 g_mass_storage.removable=1 g_mass_storage.file=/fat g_mass_storage.ro=1 g_mass_storage.idVendor=0x066F g_mass_storage.idProduct=0x37FF g_mass_storage.iSerialNumber= enable_wait_mode=off
PID hash table entries: 4096 (order: 2, 16384 bytes)
Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
Memory: 693016K/1048576K available (6895K kernel code, 319K rwdata, 2412K rodata, 388K init, 423K bss, 27880K reserved, 327680K cma-reserved, 0K highmem)
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
vmalloc : 0xc0800000 - 0xff000000 (1000 MB)
lowmem : 0x80000000 - 0xc0000000 (1024 MB)
pkmap : 0x7fe00000 - 0x80000000 ( 2 MB)
modules : 0x7f000000 - 0x7fe00000 ( 14 MB)
.text : 0x80008000 - 0x8091ef88 (9308 kB)
.init : 0x8091f000 - 0x80980000 ( 388 kB)
.data : 0x80980000 - 0x809cff00 ( 320 kB)
.bss : 0x809d2000 - 0x80a3bf14 ( 424 kB)
SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
Preemptible hierarchical RCU implementation.
Additional per-CPU info printed with stalls.
NR_IRQS:16 nr_irqs:16 16
L2C-310 erratum 769419 enabled
L2C-310 enabling early BRESP for Cortex-A9
L2C-310 full line of zeros enabled for Cortex-A9
L2C-310 ID prefetch enabled, offset 16 lines
L2C-310 dynamic clock gating enabled, standby mode enabled
L2C-310 cache controller enabled, 16 ways, 1024 kB
L2C-310: CACHE_ID 0x410000c7, AUX_CTRL 0x76070001
mxc_clocksource_init 3000000
Switching to timer-based delay loop, resolution 333ns
sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 715827882841ns
clocksource mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 637086815595 ns
Console: colour dummy device 80x30
Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
CPU: Testing write buffer coherency: ok
CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
Setting up static identity map for 0x10008280 - 0x100082f0
CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
CPU2: thread -1, cpu 2, socket 0, mpidr 80000002
CPU3: thread -1, cpu 3, socket 0, mpidr 80000003
Brought up 4 CPUs
SMP: Total of 4 processors activated (24.00 BogoMIPS).
CPU: All CPU(s) started in SVC mode.
devtmpfs: initialized
VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
clocksource jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
pinctrl core: initialized pinctrl subsystem
NET: Registered protocol family 16
DMA: preallocated 256 KiB pool for atomic coherent allocations
cpuidle: using governor ladder
cpuidle: using governor menu
CPU identified as i.MX6Q, silicon rev 1.2
anatop_regulator 20c8000.anatop:regulator-vddcore@140: Failed to read a valid default voltage selector.
anatop_regulator: probe of 20c8000.anatop:regulator-vddcore@140 failed with error -22
anatop_regulator 20c8000.anatop:regulator-vddsoc@140: Failed to read a valid default voltage selector.
anatop_regulator: probe of 20c8000.anatop:regulator-vddsoc@140 failed with error -22
hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
hw-breakpoint: maximum watchpoint size is 4 bytes.
imx6q-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
mxs-dma 110000.dma-apbh: initialized
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
2000000.aips-bus:usbphy_nop1 supply vcc not found, using dummy regulator
2000000.aips-bus:usbphy_nop2 supply vcc not found, using dummy regulator
i2c i2c-0: IMX I2C adapter registered
i2c i2c-0: can't use DMA
i2c i2c-1: IMX I2C adapter registered
i2c i2c-1: can't use DMA
i2c i2c-2: IMX I2C adapter registered
i2c i2c-2: can't use DMA
Linux video capture interface: v2.00
pps_core: LinuxPPS API ver. 1 registered
pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <[email protected]>
PTP clock support registered
imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
imx-ipuv3 2800000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
Advanced Linux Sound Architecture Driver Initialized.
Switched to clocksource mxc_timer1
NET: Registered protocol family 2
TCP established hash table entries: 8192 (order: 3, 32768 bytes)
TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
TCP: Hash tables configured (established 8192 bind 8192)
UDP hash table entries: 512 (order: 2, 16384 bytes)
UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
Trying to unpack rootfs image as initramfs...
Freeing initrd memory: 7392K (82c00000 - 83338000)
CPU PMU: Failed to parse /soc/pmu/interrupt-affinity[0]
hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available
imx rpmsg driver is registered.
Bus freq driver module loaded
futex hash table entries: 1024 (order: 4, 65536 bytes)
VFS: Disk quotas dquot_6.6.0
VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
NFS: Registering the id_resolver key type
Key type id_resolver registered
Key type id_legacy registered
jffs2: version 2.2. (NAND) c 2001-2006 Red Hat, Inc.
fuse init (API version 7.23)
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
imx-weim 21b8000.weim: Driver registered.
backlight supply power not found, using dummy regulator
mxc_sdc_fb fb@0: NO mxc display driver found!
mxc_sdc_fb fb@1: NO mxc display driver found!
mxc_sdc_fb fb@2: registered mxc display driver lcd
Console: switching to colour frame buffer device 100x30
mxc_sdc_fb fb@3: NO mxc display driver found!
imx-sdma 20ec000.sdma: no iram assigned, using external mem
imx-sdma 20ec000.sdma: no event needs to be remapped
imx-sdma 20ec000.sdma: loaded firmware 3.3
imx-sdma 20ec000.sdma: initialized
pfuze100-regulator 1-0008: Full layer: 1, Metal layer: 1
pfuze100-regulator 1-0008: FAB: 0, FIN: 0
pfuze100-regulator 1-0008: pfuze100 found.
2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 25, base_baud = 5000000) is a IMX
console [ttymxc0] enabled
imx sema4 driver is registered.
[drm] Initialized drm 1.1.0 20060810
[drm] Initialized vivante 1.0.0 20120216 on minor 0
brd: module loaded
loop: module loaded
ahci-imx 2200000.sata: fsl,transmit-level-mV not specified, using 00000024
ahci-imx 2200000.sata: fsl,transmit-boost-mdB not specified, using 00000480
ahci-imx 2200000.sata: fsl,transmit-atten-16ths not specified, using 00002000
ahci-imx 2200000.sata: fsl,receive-eq-mdB not specified, using 05000000
ahci-imx 2200000.sata: SSS flag set, parallel bus scan disabled
ahci-imx 2200000.sata: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode
ahci-imx 2200000.sata: flags: ncq sntf stag pm led clo only pmp pio slum part ccc apst
scsi host0: ahci-imx
ata1: SATA max UDMA/133 mmio [mem 0x02200000-0x02203fff] port 0x100 irq 309
m25p80 spi0.0: m25p32 (4096 Kbytes)
spi_imx 2008000.ecspi: probed
2188000.ethernet supply phy not found, using dummy regulator
pps pps0: new PPS source ptp0
libphy: fec_enet_mii_bus: probed
fec 2188000.ethernet eth0: registered PHC device 0
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ehci-mxc: Freescale On-Chip EHCI Host driver
usbcore: registered new interface driver usb-storage
2184800.usbmisc supply vbus-wakeup not found, using dummy regulator
usb_otg_vbus: supplied by SWBST
usb_h1_vbus: supplied by SWBST
ci_hdrc ci_hdrc.1: EHCI Host Controller
ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1
ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
Mass Storage Function, version: 2009/09/11
LUN: removable file: (no medium)
LUN: removable read only file: /fat
Number of LUNs=1
Number of LUNs=1
g_mass_storage gadget: Mass Storage Gadget, version: 2009/09/11
g_mass_storage gadget: g_mass_storage ready
mousedev: PS/2 mouse device common for all mice
egalax_ts 1-0004: Failed to read firmware version
egalax_ts: probe of 1-0004 failed with error -5
input: EETI eGalax Touch Screen as /devices/soc0/soc/2100000.aips-bus/21a8000.i2c/i2c-2/2-0004/input/input1
snvs_rtc 20cc000.snvs:snvs-rtc-lp: rtc core: registered 20cc000.snvs:snvs-r as rtc0
i2c /dev entries driver
IR NEC protocol handler initialized
IR RC5(x/sz) protocol handler initialized
IR RC6 protocol handler initialized
IR JVC protocol handler initialized
IR Sony protocol handler initialized
IR SANYO protocol handler initialized
IR Sharp protocol handler initialized
IR MCE Keyboard/mouse protocol handler initialized
IR XMP protocol handler initialized
imx2-wdt 20c0000.wdog: use WDOG_B to reboot.
imx2-wdt 20c0000.wdog: timeout 60 sec (nowayout=0)
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
/soc/aips-bus@02100000/usdhc@02194000: voltage-ranges unspecified
sdhci-esdhc-imx 2194000.usdhc: Got CD GPIO
sdhci-esdhc-imx 2194000.usdhc: Got WP GPIO
sdhci-esdhc-imx 2194000.usdhc: No vmmc regulator found
sdhci-esdhc-imx 2194000.usdhc: No vqmmc regulator found
mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA
/soc/aips-bus@02100000/usdhc@02198000: voltage-ranges unspecified
sdhci-esdhc-imx 2198000.usdhc: Got CD GPIO
sdhci-esdhc-imx 2198000.usdhc: Got WP GPIO
sdhci-esdhc-imx 2198000.usdhc: No vmmc regulator found
sdhci-esdhc-imx 2198000.usdhc: No vqmmc regulator found
ata1: SATA link down (SStatus 0 SControl 300)
ahci-imx 2200000.sata: no device found, disabling link.
ci_hdrc ci_hdrc.0: freeing queued request
ahci-imx 2200000.sata: pass ahci_imx..hotplug=1 to enable hotplug
mmc2: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA
/soc/aips-bus@02100000/usdhc@0219c000: voltage-ranges unspecified
sdhci-esdhc-imx 219c000.usdhc: No vmmc regulator found
sdhci-esdhc-imx 219c000.usdhc: No vqmmc regulator found
mmc3: SDHCI controller on 219c000.usdhc [219c000.usdhc] using ADMA
mmc2: new high speed SDHC card at address b368
mmcblk2: mmc2:b368 SDC 3.80 GiB
mmcblk2: p1 p2
mxc_vpu 2040000.vpu_fsl: VPU initialized
mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
g_mass_storage gadget: high-speed config #1: Linux File-Backed Storage
wm8962 0-001a: Failed to read ID register
wm8962: probe of 0-001a failed with error -5
imx-wm8962 sound: failed to find codec platform device
imx-wm8962: probe of sound failed with error -22
NET: Registered protocol family 10
sit: IPv6 over IPv4 tunneling driver
NET: Registered protocol family 17
Key type dns_resolver registered
Registering SWP/SWPB emulation handler
input: gpio-keys as /devices/soc0/gpio-keys/input/input2
snvs_rtc 20cc000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01 00:00:00 UTC (0)
VGEN3: disabling
VGEN2: disabling
VGEN1: disabling
SW4: disabling
mipi_dsi_pwr_on: disabling
sensor-supply: disabling
wm8962-supply: disabling
usb_otg_vbus: disabling
ALSA device list:
No soundcards found.
Freeing unused kernel memory: 388K (8091f000 - 80980000)
Starting UTP
uuc 0.5 [built Mar 12 2016 19:04:20]
UTP: Waiting for device to appear
UTP: file/device node /dev/utp already exists
cpu_id is 0
mmc3: new DDR MMC card at address 0001
mmcblk3: mmc3:0001 SEM08G 7.39 GiB
UTP: received command 'send'
mmcblk3boot0: mmc3:0001 SEM08G partition 1 2.00 MiB
UTP: sending Success to kernel fommcblk3boot1: mmc3:0001 SEM08G partition 2 2.00 MiB
r command send.
UTP: received commcblk3rpmb: mmc3:0001 SEM08G partition 3 128 KiB
mmand '$ tar xf $FILE '
UTP: executing "tar xf $FILE "
UTP: sending Success to kernel for command $ tar xf $FILE .
utp_poll: pass returned.
UTP: received command '$ sh mksdcard-android.sh /dev/mmcblk3'
UTP: executing "sh mksdcard-android.sh /dev/mmcblk3"
mmcblk3: card_busy_detect: error sending status cmd, status 0x80900
mmcblk3: retrying write for general error
mmcblk3: card_busy_detect: error sending status cmd, status 0x80900
mmcblk3: retrying write for general error
mmcblk3: card_busy_detect: error sending status cmd, status 0x80900
mmcblk3: retrying write for general error
mmcblk3: card_busy_detect: error sending status cmd, status 0x80900
mmcblk3: retrying write for general error
mmcblk3: card_busy_detect: error sending status cmd, status 0x80900
mmcblk3: retrying write for general error
mmcblk3: card_busy_detect: error sending status cmd, status 0x80900
mmcblk3: retrying write for general error
blk_update_request: I/O error, dev mmcblk3, sector 0
Buffer I/O error on dev mmcblk3, logical block 0, lost async page write
------------[ cut here ]------------
WARNING: CPU: 0 PID: 92 at /home2/bamboo/build/4.1.X-1.0.0_ga/fsl-imx-x11/temp_build_dir/build_fsl-imx-x11/tmp/work-shared/imx6qdlsolo/kernel-mfgtool-source/fs/block_dev.c:56 __blkdev_put+0xc4/0x1e0()
Modules linked in:
CPU: 0 PID: 92 Comm: dd Not tainted 4.1.15-1.0.0-mfgtool+g3924425 #1
Hardware name: Freescale i.MX6 Quad/DualLite (Device Tree)
[<80015ee4>] (unwind_backtrace) from [<80012774>] (show_stack+0x10/0x14)
[<80012774>] (show_stack) from [<8068fca4>] (dump_stack+0x80/0xc8)
[<8068fca4>] (dump_stack) from [<80035f5c>] (warn_slowpath_common+0x74/0xb0)
[<80035f5c>] (warn_slowpath_common) from [<80036034>] (warn_slowpath_null+0x1c/0x24)
[<80036034>] (warn_slowpath_null) from [<8011abc8>] (__blkdev_put+0xc4/0x1e0)
[<8011abc8>] (__blkdev_put) from [<8011b194>] (blkdev_close+0x18/0x20)
[<8011b194>] (blkdev_close) from [<800ebf28>] (__fput+0x80/0x1c8)
[<800ebf28>] (__fput) from [<8004cf0c>] (task_work_run+0xb4/0xe8)
[<8004cf0c>] (task_work_run) from [<80012394>] (do_work_pending+0x7c/0xa4)
[<80012394>] (do_work_pending) from [<8000f50c>] (work_pending+0xc/0x20)
---[ end trace 7127830681579d6b ]---
1+0 records in
1+0 records out
1024 bytes (1.0 kB) copied, 0.183692 s, 5.6 kB/s
Checking that no-one is using thirandom: sfdisk urandom read with 12 bits of entropy available
s disk right now ... OK

Disk /dev/mmcblk3: 7.4 GiB, 7944011776 bytes, 15515648 sectors
Units: sectors of 1 * 512 = 512 bytes
Sector size (logical/phmmcblk3: card_busy_detect: error sending status cmd, status 0x80900
ysical): 512 bytes / 512 bytes
Immcblk3: retrying write for general error
/O size (minimum/optimal): 512 bymmcblk3: card_busy_detect: error sending status cmd, status 0x80900
tes / 512 bytes

>>> Created a mmcblk3: retrying write for general error
new DOS disklabel with disk identmmcblk3: card_busy_detect: error sending status cmd, status 0x80900
ifier 0xc7d10649.
Created a new mmcblk3: retrying write for general error
partition 1 of type 'Linux' and ommcblk3: card_busy_detect: error sending status cmd, status 0x80900
f size 24 MiB.
/dev/mmcblk3p2: Cmmcblk3: retrying write for general error
reated a new partition 2 of type mmcblk3: card_busy_detect: error sending status cmd, status 0x80900
'Linux' and of size 16 MiB.
/devmmcblk3: retrying write for general error
/mmcblk3p3: Created a new partitimmcblk3: card_busy_detect: error sending status cmd, status 0x80900
on 3 of type 'Extended' and of simmcblk3: retrying write for general error
ze 1.3 GiB.
/dev/mmcblk3p4: Creablk_update_request: I/O error, dev mmcblk3, sector 2807808
ted a new partition 4 of type 'LiBuffer I/O error on dev mmcblk3, logical block 350976, lost async page write
nux' and of size 6 GiB.
/dev/mmcmmcblk3: card_busy_detect: error sending status cmd, status 0x80900
blk3p5: Created a new partition 5mmcblk3: retrying write for general error
of type 'Linux' and of size 800 mmcblk3: card_busy_detect: error sending status cmd, status 0x80900
MiB.
/dev/mmcblk3p6: Created a nmmcblk3: retrying write for general error
ew partition 6 of type 'Linux' anmmcblk3: card_busy_detect: error sending status cmd, status 0x80900
d of size 512 MiB.
/dev/mmcblk3pmmcblk3: retrying write for general error
7: Created a new partition 7 of tmmcblk3: card_busy_detect: error sending status cmd, status 0x80900
ype 'Linux' and of size 8 MiB.
/mmcblk3: retrying write for general error
dev/mmcblk3p8: Created a new partmmcblk3: card_busy_detect: error sending status cmd, status 0x80900
ition 8 of type 'Linux' and of simmcblk3: retrying write for general error
ze 6 MiB.
/dev/mmcblk3p9: Createmmcblk3: card_busy_detect: error sending status cmd, status 0x80900
d a new partition 9 of type 'Linummcblk3: retrying write for general error
x' and of size 2 MiB.
/dev/mmcblblk_update_request: I/O error, dev mmcblk3, sector 2793472
k3p10:
New situation:

DeBuffer I/O error on dev mmcblk3, logical block 349184, lost async page write
vice Boot mcblk3: card_busy_detect: error sending status cmd, status 0x80900
m Start End mcblk3: retrying write for general error
m Sectors Size Immcblk3: card_busy_detect: error sending status cmd, status 0x80900
d Type
/dev/mmcblk3pmmcblk3: retrying write for general error
1 2048 51199 49152 mmcblk3: card_busy_detect: error sending status cmd, status 0x80900
24M 83 Linux
/dev/mmcblk3p2 mmcblk3: retrying write for general error
51200 83967 32768 16mmcblk3: card_busy_detect: error sending status cmd, status 0x80900
M 83 Linux
/dev/mmcblk3p3 mmcblk3: retrying write for general error
83968 2885631 2801664 1.3G 5mmcblk3: card_busy_detect: error sending status cmd, status 0x80900
Extended
/dev/mmcblk3p4 28mmcblk3: retrying write for general error
85632 15515647 12630016 6G 83 mmcblk3: card_busy_detect: error sending status cmd, status 0x80900
Linux
/dev/mmcblk3p5 8601mmcblk3: retrying write for general error
6 1724415 1638400 800M 83 Linublk_update_request: I/O error, dev mmcblk3, sector 2775040
x
/dev/mmcblk3p6 1726464 2Buffer I/O error on dev mmcblk3, logical block 346880, lost async page write
775039 1048576 512M 83 Linux
/mmcblk3: card_busy_detect: error sending status cmd, status 0x80900
dev/mmcblk3p7 2777088 27934mmcblk3: retrying write for general error
71 16384 8M 83 Linux
/dev/mmcblk3: card_busy_detect: error sending status cmd, status 0x80900
mmcblk3p8 2795520 2807807 mmcblk3: retrying write for general error
12288 6M 83 Linux
/dev/mmcbmmcblk3: card_busy_detect: error sending status cmd, status 0x80900
lk3p9 2809856 2813951 4mmcblk3: retrying write for general error
096 2M 83 Linux

Partition tmmcblk3: card_busy_detect: error sending status cmd, status 0x80900
able entries are not in disk ordemmcblk3: retrying write for general error
r.

The partition table has beemmcblk3: card_busy_detect: error sending status cmd, status 0x80900
n altered.
mmcblk3: retrying write for general error
mmcblk3: card_busy_detect: error sending status cmd, status 0x80900
mmcblk3: retrying write for general error
blk_update_request: I/O error, dev mmcblk3, sector 0
Buffer I/O error on dev mmcblk3, logical block 0, lost async page write
mmcblk3: card_busy_detect: error sending status cmd, status 0x80900
mmcblk3: retrying write for general error
mmcblk3: card_busy_detect: error sending status cmd, status 0x80900
mmcblk3: retrying write for general error
mmcblk3: card_busy_detect: error sending status cmd, status 0x80900
mmcblk3: retrying write for general error
mmcblk3: card_busy_detect: error sending status cmd, status 0x80900
mmcblk3: retrying write for general error
mmcblk3: card_busy_detect: error sending status cmd, status 0x80900
mmcblk3: retrying write for general error
mmcblk3: card_busy_detect: error sending status cmd, status 0x80900
mmcblk3: retrying write for general error
blk_update_request: I/O error, dev mmcblk3, sector 83968
Buffer I/O error on dev mmcblk3, logical block 10496, lost async page write
mmcblk3: card_busy_detect: error sending status cmd, status 0x80900
mmcblk3: retrying write for general error
mmcblk3: card_busy_detect: error sending status cmd, status 0x80900
mmcblk3: retrying write for general error
mmcblk3: card_busy_detect: error sending status cmd, status 0x80900
mmcblk3: retrying write for general error
mmcblk3: card_busy_detect: error sending status cmd, status 0x80900
mmcblk3: retrying write for general error
mmcblk3: card_busy_detect: error sending status cmd, status 0x80900
mmcblk3: retrying write for general error
mmcblk3: card_busy_detect: error sending status cmd, status 0x80900
mmcblk3: retrying write for general error
blk_update_request: I/O error, dev mmcblk3, sector 1724416
Buffer I/O error on dev mmcblk3, logical block 215552, lost async page write
Calling ioctl() to re-read partition table.
/dev/mmcblk3: close device failed: Input/output error
sfdisk: /dev/mmcblk3: cannot modify partition 1: no partition table was found
formating android data partition
mke2fs 1.42.9 (28-Dec-2013)
Could not stat /dev/mmcblk3p4 --- No such file or directory

The device apparently does not exist; did you specify it correctly?
UTP: sending Non-success to kernel for command $ sh mksdcard-android.sh /dev/mmcblk3.
utp_poll: exit with status 256

What could I do in the state?

Thank you with your help.

Have a great day,

Yen

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

2,157件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

You can use the IMX6_M6.0.1_2.1.0_MFG_TOOL version mfgtool to download the images to your emmc. Use the mfgtool2-android-mx6q-sabresd-emmc.vbs file.

Hope this can do help for you.

Have a nice day

Rita

0 件の賞賛
返信

2,157件の閲覧回数
yenchou
Contributor III

Hi Rita,

Thank you for your help.

I forgot to say I used the  IMX6_M6.0.1_2.1.0_MFG_TOOL version mfgtool.

So it should not be this problem.

Have a great day,

Yen

讚 (0) 

0 件の賞賛
返信