Mfgtool abnormal exit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Mfgtool abnormal exit

1,759 Views
mokey
Contributor I

hello:

            Now use the code imx6q Android8.0, download the firmware and tool from the official website, open the Mfgtool tool, power the board, plug in the USB, Mfgtool abnormal exit。

log

DLL version: 2.7.0
Tuesday, October 16, 2018 10:22:31   Start new logging
ModuleID[2] LevelID[10]: CMyExceptionHandler thread is running
ModuleID[2] LevelID[1]: new MxHidDeviceClass
ModuleID[2] LevelID[10]: new MxHidDevice[01359DD0]
ModuleID[2] LevelID[1]: new MxHidDeviceClass
ModuleID[2] LevelID[10]: new MxHidDevice[0135A278]
ModuleID[2] LevelID[1]: new MxHidDeviceClass
ModuleID[2] LevelID[10]: new MxHidDevice[0588E7A0]
ModuleID[2] LevelID[1]: new MxHidDeviceClass
ModuleID[2] LevelID[10]: new MxHidDevice[0588EB40]
ModuleID[2] LevelID[1]: new MxHidDeviceClass
ModuleID[2] LevelID[10]: new MxHidDevice[0588F220]
ModuleID[2] LevelID[1]: new MxHidDeviceClass
ModuleID[2] LevelID[10]: new MxHidDevice[01358DD0]
ModuleID[2] LevelID[1]: new MxHidDeviceClass
ModuleID[2] LevelID[10]: new MxHidDevice[0590E850]
ModuleID[2] LevelID[1]: new MxHidDeviceClass
ModuleID[2] LevelID[10]: new MxHidDevice[0590EB30]
ModuleID[2] LevelID[1]: new MxHidDeviceClass
ModuleID[2] LevelID[10]: new MxHidDevice[013594B0]
ModuleID[2] LevelID[10]: Device Manager thread is running
ModuleID[2] LevelID[1]: Can't set m_hStopEvent before it initialized or it already stop
Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

1,652 Views
张松源
Contributor III

hi  mokey one,   

have you solve this problem, please tell me the way.  I was using  imx6sl Android8.0.

0 Kudos
Reply

1,652 Views
igorpadykov
NXP Employee
NXP Employee

Hi mokey

detailed description of mfg tool usage is provided in Android_Quick_Start_Guide.pdf provided with package,

also one can check if correct package was used and try to test with i.MX6Q Sabre SD reference board:

i.MX 6/7D Series Manufacturing Toolkit for Android O8.0.0_1.0.0 Release

https://www.nxp.com/webapp/Download?colCode=IMX_O8.0.0_1.0.0_TOOL&appType=license&location=null&Pare... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply