Mfgtool abnormal exit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Mfgtool abnormal exit

1,751件の閲覧回数
mokey
Contributor I

hello:

            Now use the code imx6q Android8.0, download the firmware and tool from the official website, open the Mfgtool tool, power the board, plug in the USB, Mfgtool abnormal exit。

log

DLL version: 2.7.0
Tuesday, October 16, 2018 10:22:31   Start new logging
ModuleID[2] LevelID[10]: CMyExceptionHandler thread is running
ModuleID[2] LevelID[1]: new MxHidDeviceClass
ModuleID[2] LevelID[10]: new MxHidDevice[01359DD0]
ModuleID[2] LevelID[1]: new MxHidDeviceClass
ModuleID[2] LevelID[10]: new MxHidDevice[0135A278]
ModuleID[2] LevelID[1]: new MxHidDeviceClass
ModuleID[2] LevelID[10]: new MxHidDevice[0588E7A0]
ModuleID[2] LevelID[1]: new MxHidDeviceClass
ModuleID[2] LevelID[10]: new MxHidDevice[0588EB40]
ModuleID[2] LevelID[1]: new MxHidDeviceClass
ModuleID[2] LevelID[10]: new MxHidDevice[0588F220]
ModuleID[2] LevelID[1]: new MxHidDeviceClass
ModuleID[2] LevelID[10]: new MxHidDevice[01358DD0]
ModuleID[2] LevelID[1]: new MxHidDeviceClass
ModuleID[2] LevelID[10]: new MxHidDevice[0590E850]
ModuleID[2] LevelID[1]: new MxHidDeviceClass
ModuleID[2] LevelID[10]: new MxHidDevice[0590EB30]
ModuleID[2] LevelID[1]: new MxHidDeviceClass
ModuleID[2] LevelID[10]: new MxHidDevice[013594B0]
ModuleID[2] LevelID[10]: Device Manager thread is running
ModuleID[2] LevelID[1]: Can't set m_hStopEvent before it initialized or it already stop
ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,644件の閲覧回数
张松源
Contributor III

hi  mokey one,   

have you solve this problem, please tell me the way.  I was using  imx6sl Android8.0.

0 件の賞賛
返信

1,644件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi mokey

detailed description of mfg tool usage is provided in Android_Quick_Start_Guide.pdf provided with package,

also one can check if correct package was used and try to test with i.MX6Q Sabre SD reference board:

i.MX 6/7D Series Manufacturing Toolkit for Android O8.0.0_1.0.0 Release

https://www.nxp.com/webapp/Download?colCode=IMX_O8.0.0_1.0.0_TOOL&appType=license&location=null&Pare... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信