MfgTool repeat the burning process

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MfgTool repeat the burning process

2,730 Views
xixiguohan
Contributor II

If I don't click stop button, MfgTool will repeat the burning process. Is that normal?

Why can't it stop automatically after xml commands are all executed?

0 Kudos
Reply
5 Replies

2,649 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

And then check your hardware design refer to the reference design.

0 Kudos
Reply

2,649 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

When you use the mfgtool do download the images to your board, after success download, it will stop automatically and you can see download successful done. Here you need to check the setting of mfgtool first.

0 Kudos
Reply

2,649 Views
xixiguohan
Contributor II

Hi Rita,

After download complete, the MfgTool window displayed this.

pastedImage_1.png

Yes, this means download successsfully, but if I don't click "Stop" button, and Exit, it will repeat to download the images after about 3 minutes.

Do you know where to set the MfgTool configurations to stop the repeat download?

0 Kudos
Reply

2,649 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Which board and BSP are you using? When download complete, I will click the stop button and exit.

Is your board designed yourself?

0 Kudos
Reply

2,649 Views
xixiguohan
Contributor II

My board is customized based on imx6sl, and BSP is customized based on Yocto. But I think this has nothing to do with my board and BSP. You can try not click the stop button, and wait for about 4 minutes. Check if it will going to happen on your board.

0 Kudos
Reply